Solid Edge Centre of Mass symbol does not update in Drawing View after physical properties suppressed

2021-10-06T23:59:05Z
DRAFT

Summary


Details

The user has an assembly; all the components have a material assigned.  In Inspect - Physical Properties they turn on 'Display symbol' for Center of Mass (CoM). 


The green dot indicating the CoM is displayed.


The user then creates a drawing of the assembly.  In the Drawing View properties - Display - they select the Center of Mass and activate 'Show'.



The CoM symbol is displayed.
In the assembly the user opens Occurrence Properties and sets the Physical properties to 'No' for the radiator.  Accordingly, the CoM will update to a new position. 

Returning to the drawing - the Drawing View is shown as out of date.  The user updates it expecting the CoM symbol to update its position, but it does not.

Solution

Currently, update of the CoM symbol is not supported in a drawing when the Physical properties of some components in the assembly are set to 'No' in Occurrence Properties.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V221.0
Function: DRAWING_VIEWS

Ref: 002-8567226

KB Article ID# PL8567226

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS