"Unite" command can be established with just the "tool body"

2021-10-06T23:28:06Z

Summary


Details

When trying to execute Unite command, selecting both of Target and Tool is required. If those two are not selected, Unite command cannot be applied due to No OK or Apply button is available to finish the command. 


However, when editing the Unite command, the command succeeds even if no target is selected. It means succeeding the function if the target is released.


Reproduced Steps:


1.Creates 2 solid bodies
2.Executing Unite command

3.Go to edit the Unite feature > release the target > OK


Solution

The behavior is working as expected.


When user launches the dialog to create Unite Feature, target must be provided. 


However, if user edits that feature, target can be changed or deselected. Because we hope to make the Unite Feature more robust during edit or update.


The picture below shows a case where three Booleans are created by one time operation of Unite command, and two of the three created bodies do not have tools.


Notes and References

*** Please refer to PL8566979 for Japanese article.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1953
Function: FEATURE_MODEL

Ref: 002-8566980

KB Article ID# PL8566980

Contents

SummaryDetails

Associated Components