How to detect non-intersecting "Unite" features

2021-10-06T23:28:06Z

Summary


Details

Due to the enhancement that allows to generate multiple bodies by "Unite" command, as a result, it is not possible to determine whether the body created by the command is a single body or multiple bodies. Is there any function to detect it?

Reproduced Steps:


1.Create multiple bodies which has no intersection such as below.
2.Execute "Unite" command


Solution

You can detect whether the created body is a single or not by Check Mate command.


1.HD3D tool > "Check-Mate" > "Set Up Tests> "Tests"> "Get Information">"Modeling">"Report Boolean Features that Generate Multiple Bodies"


Notes and References

*** Please refer to PL8566975 for Japanese article.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1953
Function: FEATURE_MODEL

Ref: 002-8566976

KB Article ID# PL8566976

Contents

SummaryDetails

Associated Components