How to transfer the formatted columns in the Design Manager to another system?

2021-10-06T23:59:03Z

Summary


Details

The user customizes the columns in the Design Manager via the 'Format Columns' dialog and wants to transfer these setting to another system. How can this be executed?

Solution

This task can be achieved via the following steps from the source to the respective target system.

Source system:


  • Run the 'Registry Editor' command
  • Expand to Computer\HKEY_CURRENT_USER\SOFTWARE\Siemens\Solid Edge\Version 221\General\DesignManager
  • Select the folder DesignManager
  • Select 'File > Export...'
  • Define a 'File name' (e.g. SE-DesignManager.reg)
  • 'Save' the file
  • Exit the 'Registry Editor' session

Target system:


  • Run the 'Registry Editor' command
  • Select 'File > Import...'
  • Select the reg file that was previously created in the sources system (e.g. SE-DesignManager.reg)
  • 'Open' the file.
  • Quit the message "The keys and values contained in ... have been successfully added to the registry." with OK.
  • Exit the 'Registry Editor' session

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: DESIGN_MANAGER

Ref: 002-8566083

KB Article ID# PL8566083

Contents

SummaryDetails

Associated Components