How to show Mass value in Teamcenter Item Rev properties form?
2021-10-06T23:28:05Z
Summary
Details
How to show Mass value in Teamcenter Item Rev properties form?
Solution
These are the required steps to configure:
In BMIDE: (1) Create a custom item type "AU54GTACITEM"(2) Open the AU54GTACITEMRevision (3) Select the Properties tab. (4) Add a new Compound property. (5) Property Type = Compound. Select 'Next'. (6) Enter a name, for example: au54_mass (7) Enter a Display name: au54_mass (8) Enter the Description: Mass (9) Select the top line of the Path and select 'Add Segment'. (10) Select IMAN_specification -> Next. (11) Select UGMASTER -> Finish. (12) Select the second (UGMASTER) line of the Path and select 'Add Segment'. (13) Select ref_list -> Next. (14) Select UGPartMassPropsForm -> Finish. (15) Select the last (UGPartMassPropsForm) line of the Path and select 'Add Final Segment'. (16) Select mass -> Finish. (17) Select 'Finish' to create the compound property. (18) Save the data model and deploy.
Attribute Mapping File: (1) Build this mapping under UGMaster
(2) Save and import the mapping file back into TC.
In NX: (1) Launch new Session of TC and NX. (2) In NX, Create a new item using the above custom item type (3) Add any solid body into the file. (4) Go to "File > Properties". (5) Select the "Mass" tab (6) You may want to consider toggle on the option, "Update Mass Properties on Save" so that mass is updated when the part is saved. (7) Select the "Update Mass Properties Now" icon (circular arrow). This will put weight data into the part. (8) 'OK' the Properties dialog. (9) Save the file. (10) Select "File > Properties". Select the 'Attributes' tab. (11) Notice MassPropMass attribute exists, and has a value.
In TC: (1) On the Item Revision of above saved file, RMB > View Properties, click "All" to see all properties, and the bottom of the list will show that BMIDE created compound property "au54_mass", its value matches the MassPropMass in NX.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: NXMANAGER Version: V1957 Function: ATTRIBUTES