How to display "Properties" in [New] Dialog?

2021-10-06T23:28:05Z

Summary


Details

How to display "Properties" in [New] Dialog?
Properties are not displayed as shown below.





Steps to reproduce the problem-


Run in TCIN environment.


(1) Select [File]-[New]-[Item]


(2) Confirm Dialog. Properties is not displayed


Similarly, "Properties" is not displayed on NX 1980 in the TCIN environment.


However, "Properties" is displayed on NX 10.0.3.5 in the TCIN environment.




Also, the "Properties" is displayed on NX 1953 in a Native environment.






Solution

Currently, this is working as a design. All these properties are now added to the Column Configuration in the NX File > New Dialog. Refer to the below snapshot.


Notes and References

10120996



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1953
Function: FILE_NEW

Ref: 002-8565482

KB Article ID# PL8565482

Contents

SummaryDetails

Associated Components