Solid Edge SEEC Save As user interface shows inconsistent Solid Edge Property Real Name on CPD

2021-10-06T23:59:01Z
DOC_MANAGEMENT

Summary


Details

SEEC Save As user interface shows inconsistent Solid Edge Property Real Name on CPD

Solution

If the custom property is both mapped as well as is part of the create descriptor in BMIDE, 


in such case SEEC gives precedence to create descriptor property while saving the new file.

Hence it will be shown in the first row on CPD.

If the property is only mapped property it will be shown in second row on CPD.

This is designed behavior.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221MP6
Function: SEEC

Ref: 002-8565445

KB Article ID# PL8565445

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC