Details
The NX assembly Structure was found to be out of sync with the Teamcenter BOM View.
1. Create a assembly with customer default "Structure Update on Save" ON.
2. Save the assembly.
3. Disable "Structure Update on Save" in customer defaults and restart NX
4. Modify the assembly
5. Now export the same assembly using Export Assembly outside Teamcenter
Below warning is displayed
++++++++++++++++++++++++
Assembly Load for Export Warning
The NX assembly structure was found to be out of sync with the Teamcenter BOM View for the following parts
XXXXXX/A;1
If you choose to continue, the BOM views created for clones of these parts will be out of sync with the NX assembly structure.
Solution
During load TCIN compares the "last_struct_mod" date in the BVRSyncInfo form to the "Structure Last Modified" date of the BOMView.
If the last sync date is out of date then warning will be displayed during export.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1930
Function: CLONE_EXPORT
Ref: 002-8565105