NX Attribute value in NX is not same as Teamcenter

2021-10-06T23:28:04Z
NX for Design

Summary


Details

If the attribute value is "empty or null" in Teamcneter then NX is showing the previously saved attribute value. 

Solution

To display "Empty" or "Null" value of the attribute in NX, user needs to add "/allow_null_value" in the attribute mapping file then only the value is updated.

Ex:
MASS : NR(UGPART-MASSPR).mass /master=none /description="Mass (kg)" /allow_null_value 



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1926
Function: ATTRIBUTES

Ref: 002-8565092

KB Article ID# PL8565092

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX