How to create a vent hole in Mold Wizard?

2021-10-06T23:28:04Z

Summary


Details

How to create a vent hole in Mold Wizard?

Solution

Solution : 

Step 1: Choose Mold Wizard tab→ Main group→ Vent.
Step 2: In the Vent dialog box, from the type list, select Standard Vent.
Step 3: In the Definition group, specify a direction in which you want to make a vent depth.
Step 4: Select reference objects as one or more parting line edges, guide curves, and then solid bodies are generated and subtracted from the Mold body.
Step 5: Select type as Single. 
Step 6: In the Details box, select a Section as Block or cylinder.
Step 7 In the Details box, Change the parameter as required.
Step 8: In the Settings group, in the Output box, select a Vent.
Step 9: Click Ok.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: KDA
Version: V1980
Function: MOLDWIZARD

Ref: 002-8564621

KB Article ID# PL8564621

Contents

SummaryDetails

Associated Components