How to delete project from the list in Solid Edge Wiring and Harness Design (SEWHD)?

2021-10-06T23:58:59Z

Summary


Details

How to delete project in SEWHD which I don't need anymore it from the list?





Solution

You can delete a project from the database when you no longer require it.

CAUTION:
The deletion of a project cannot be undone without recourse to a database backup, which may not be up-to-date.

Procedure:
1. Open the project you want to delete.
2. Press Space Bar and enter Delete Project.
3. A message is displayed asking you to confirm the deletion. Click Yes to proceed and delete the project. The project is removed from the database.

Notes and References

9937036

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V220.0
Function: DESIGN

Ref: 002-8564567

KB Article ID# PL8564567

Contents

SummaryDetails

Associated Components