Details
Unable to locate other parts edge in sketch while in-place activated and working within the context of an assembly.
Solution
The Peer Edge Locate command makes edges of other parts in locatable or non-locatable in a sketch window, and while in-place activated and working within the context of an assembly.
This command is available in Sketch Window-Tools-Edge Locate
Note:
The Peer Edge Locate command setting will remain set during a Solid Edge session and will reset to off when Solid Edge is restarted.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V221.0
Function: OTHER
Ref: 002-8564550