How can I collect settings from one machine and deploy in other?

2021-10-06T23:58:58Z

Summary


Details

How can I collect settings from one machine and deploy in other? 

Solution

You can capture settings and preferences using the Settings and Preferences Wizard.

After you capture the settings and preferences, you can deploy them to other machines using Deploy custom settings and preferences. 

1. When Solid Edge is not running, choose Start→Siemens Solid Edge 2021→Settings and Preferences Wizard.
2. Select Capture Settings and Preferences.
3. Click Next.
The Choose a location and filename box displays the default location for the settings and preferences file. You can save this file to any folder on your local machine or to a network location so you can access it from different machines.
Solid Edge also displays this location in the Solid Edge Options dialog box→File Locations tab→File types list, in the Settings and Preferences File entry.
4. Do one of the following:
 -To accept the default location:
a. Select the types of settings and preferences you want to capture.
b. Click Finish.
- To modify the location:
a. Click Browse and choose a new location.
b. Select the types of settings and preferences you want to capture.
c. Click Finish.
5. To deploy the settings and preferences to other machines, continue with Deploy custom settings and preferences.

Note: Using this uer can capture
• Registry settings—Stores many of the user preferences and customizations.
• Files from the AppData folder—Stores customized themes.
• Files from the Preferences folder—Often stored on a server, accessed by multiple users.
• Template files—Often stored on a server, accessed by multiple users.



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Function: OTHER

Ref: 002-8564547

KB Article ID# PL8564547

Contents

SummaryDetails

Associated Components