== Compare the Customer Default between NX 1980 and NX 1953==
==Also changed Mass Properties Options in NX 1980==
Solution
Each level of accuracy we used behind are as:
Standard = 0.99 Fine = 0.999 Ultra Fine = 0.9999
Notes and References
The changes in NX1980 is based on our investigation that three levels of accuracy are good enough, so since NX1980 we reduced the accuracy options to 3 and represents them as words to users.
*** Please refer to PL8564444 for Japanese article.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DESIGN Version: V1980 Function: INFO_ANALYSIS