Reattaching retained dimensions requires the origin to be redefined
2021-10-06T23:28:04Z
Summary
Details
Reattaching retained dimensions requires the origin to be redefined.
Solution
If the Auto-Alignment is set to Off or Non-Associative when the dimension is created, the associative origin won't be created and thus won't cause a retained dimension to have the need for the origin to be redefined. This is available on all dimension commands in the Origin group under Alignment.
Notes and References
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: DRAFTING Version: V1953 Function: DIMENSION