Multi-sheet Solid Edge w/SEEC drawings to PDF

2021-10-06T23:58:56Z

Summary


Details

Multi-sheet Solid Edge draft files only show as a single sheet in Teamcenter and AWS. The preview auto generated (EMF) and the auto generated PDF only seem to show the last sheet that was opened when saving the draft file. Is there a setting somewhere that needs to be changed?

Solution

1) Create NEW or open a draft file from the training folder. 
Select the SE Application Button Save As, then select Save As Translated 

2) On the Save as Translated Dialog select the PDF translate file type and press the options button. 
Now select "All sheets" radio button and OK the form. Then you can cancel the PDF file creation.


3) You are now ready to log in to Teamcenter with SEEC. Automatic PDF file creations will now include the multiple sheets of the draft file. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: xp64-sp2
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 001-10128416

KB Article ID# PL8563859

Contents

SummaryDetails

Associated Components