How can I create an NX Syslog file to be uploaded to Support Center ?
2021-10-06T23:28:04Z
Summary
Details
How can I create an NX Syslog file to be uploaded to Support Center when I have an issue (IR) ?
Solution
Here the correct procedure :
1) Exit NX 2) start NX 3) File/Open xxx.prt if ERROR : please capture error in a JPG and upload it. 4) Menu/Help/Log File 5) File Save As : IR_NUMBER.txt 6) compress it into IR_NUMBER_logs.7z 7) upload into Support Center as Commercial Unrestricted (if Data is not Military or Strictly Confidential) : IRNUMBER_logs.7z
Here an example :
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: XP64_SP2 Product: NX Application: SYSTEM Version: V1973 Function: SYSTEM_TOOLS