Buildpacks parameter is missing from manifest file.

2021-09-07T12:01:02Z

Summary


Details

The manifest file from your application in Operator Cockpit is missing the buildpacks parameter. In addition, you are unable to auto deploy your application.

Solution

The buildpacks parameter is removed from the manifest file by MindSphere if it is used when uploading your application to the Developer Cockpit by the time it becomes available in the Operator Cockpit. The auto-deployment option also becomes disabled as it does not support the buildpacks parameter.

However, you can still deploy your application by following these steps:

  1. Download your application from the Operator Cockpit.
    1. Unzip your application and add the "buildpacks" parameter in the manifest file.
      1. Finally, use manual deployment via Cloud Foundry CLI.

        For step by step instructions on manual deployment, visit:

        https://documentation.mindsphere.io/resources/html/operator-cockpit/en-US/113648908811.html

        Notes

        KB Article ID# PL8561823

        Contents

        SummaryDetails

        Associated Components