Even when I create new explosion and cancel the dialog, it is not cancelling.

2021-10-06T23:28:03Z

Summary


Details

When we try to create new explosions and cancel, the explosion name still explains in the dialog.
Assembly - Explosions - New Explosion.
Even if I cancel the "Edit Explosion" dialog and exit, the explosion is still created in the "Explosions" dialog.


When I "Cancel" the Edit Explosion dialog, I think that the specified name should not remain.

Solution

The new explosion gets created when user performs "New Explosion" action button in the explosion UI. So once the new explosion got created, most likely the user workflow would be editing the explosion. This is why "Edit Explosion" dialog opens up for user automatically, 
This is intended design. Cancelling edit explosion, would cancel just the edit operation (of the explosion).
If user doesn't want to see the explosion he created, he can delete it in explosion UI or Undo the operation.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1903
Product: NX
Application: ASSEMBLIES
Version: V1980
Function: ASSEMBLY_MODEL

Ref: 002-8561557

KB Article ID# PL8561557

Contents

SummaryDetails

Associated Components