Solid Edge Standard Parts – Creating Custom Pipes

2021-10-06T23:58:53Z

Summary


Details

The goal is to add a custom pipe component to the Solid Edge Standard Parts library that can be used with the XpresRoute – Piping Route utility.

Solution

Preparation: 

1. First create a base profile you will use to build your custom pipe category. The base feature is Ordered and always an Extrude (not a revolved extrude!). Save it with a name that will help you recognize the pipe e.g. Dairy Pipe_BS4825_127x16.par.
 

2. Start the PreparePipingComponents.exe macro to prepare your pipe.


3. Use the Prepare Pipe option and define the input and output diameter and select the two pipe openings. This utility will add the coordinate systems required for the library and will add a variable "LL" and "Diameter_1" to control the dimensions. 
 
 

KB Article ID# PL8561422

Contents

SummaryDetails

Associated Components