Solid Edge How to change the offset of the dimension measurement line from the object being measured.

2021-10-06T23:58:53Z
DRAFT

Summary


Details

How to change the offset of the dimension measurement line from the object being measured. 



Solution

This is controlled by the Element Gap, which is available on the "Lines and Coordinate" tab of the Modify Dimension Style and Dimension Properties dialogs. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V221.0
Function: DIMENSIONS

Ref: 001-10121570

KB Article ID# PL8561387

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS