Customer has a Simulation Standard license plus Solid Edge Foundation and they would like to use the
"Unite Bodies" command in Simulation Geometry - > Surfaces but the command is greyed out:
This is because there is no valid license for the command to be active. Which license is needed to make the command active?
Solution
The command is included with a Solid Edge Premium License. Otherwise the customer will need either a Solid Edge Foundation or Solid Edge Classic license plus the Solid Edge Advanced Simulation as an add on e,g,
After that the command is activated:
NotesIf you have further inquiries about Solid Edge Solid Edge Portfolio Products Licensing please refer to the FAQs Collection link below:
Solid Edge Portfolio Products Licensing FAQs Collection