Standard Parts – Teamcenter configuration and setup

2021-10-06T23:58:52Z

Summary


Details

This document will help you understand the Solid Edge Standard Parts setup and configuration with Teamcenter working with a centralized database on a network server and using the Teamcenter SQL database.

Prerequisites

A running Teamcenter environment, Teamcenter client, Solid Edge and Solid Edge Embedded Client on your workstation.



Solution

Installation of the Standard parts Administrator

On the server create a shared location for the Standard Parts
From the client check you permission, open the network location in the Windows Explorer and create a new file.  If you are able to create a new file you have sufficient permissions.
Install Standard Parts on the workstation you want to use for remote Standard Parts administration.  When prompted for the installation location, specify a UNC folder that is accessible from this workstation (for example, \\DECGNVCTC1\StandardParts, as shown the image below).
This will install the Standard Parts structure and the master parts (free example files) to the shared location.
Configure SQL server

If you have a running SQL server you can use this for Standard Parts.

1) Start SQL Server Management Studio and change the authentication mode of the database to Mixed Mode (SQL Server and Windows Authentication) in the database properties:

2) Create a login for external users that uses SQL Server authentication.
• In the Object Explorer, expand Security > Logins.
• Right-click Logins, and on the shortcut menu, choose New Login.
Username: SPUser
Password: spuser

3) Grant database creation privileges to the user
• On the New Login dialog box, click the Server Roles page.
• In the Server Roles list, set the dbcreator option.
• Click OK on all dialogs to accept the changes

Setup Configuration Wizard

Launch the Solid Edge Standard Parts Configuration Wizard.
Browse for the working databases end connect to a "External network database".

KB Article ID# PL8561032

Contents

SummaryDetails

Associated Components