"Hole clearance check has been violated" warning message being generated.

2021-10-06T23:58:50Z

Summary


Details

When placing a wire clamp, getting an error message, "Hole clearance check has been violated".



Solution

In the case of a cable or bundle, Solid Edge totals up all of the wires in the wiring harness and checks to see that there is enough room for all of the wires to fit through the hole.  A larger clamp for the wires should be chosen when receiving this error. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1511
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V221.0
Function: OTHER

Ref: 001-10116120

KB Article ID# PL8559887

Contents

SummaryDetails

Associated Components