Embedded database has crashed and Solid Edge Electrical Manager cannot connect

2021-10-06T23:58:50Z

Summary


Details

Client connections fail with popup window: "Connection Failed - Could not connect to Solid Edge Electrical Manager. Application terminated"


The Manager server crashed. Unable to start Manager service. When an attempt is made to re-start the service, it runs and then stops by itself. The Manager log file states that it can't connect to the database



Solution

The server crash has corrupted the postmaster.pid lock file. The postmaster.pid file gets created when the embedded database is started. It gets deleted when the database is stopped. When a server crashes the .pid remains and it causes a problem.


To fix this problem:


  1. Ensure the Embedded Database windows service is stopped
  2. Delete the file [Solid Edge Wiring and Harness Design Home directory]\embeddeddata\data\postmaster.pid 
  3. Re-start all services
  

Notes and References

You won't see the postmaster.pid file there though, until there is an issue with a db crash. 

Hardware/Software Configuration

Platform: all
OS: n-a
OS Version: n-a
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V221MP7
Function: OTHER

Ref: 002-8559773

KB Article ID# PL8559773

Contents

SummaryDetails

Associated Components