No relationship between NX Sheet Metal Material Library and NX Modeling Material Library
Solution
Starting NX 1953 Series, Integration of Material Library is now effective.
Once you have selected a Material in the Sheet Metal Preferences (Aluminium 2014 here),
and the Physical Material Library Integration is checked ON:

The same Material will be automatically selected in the Modeling Material Libray
when a correspondance is found:

The name of the column in ./UGII/materials/sheet_metal_material_table.txt is PHYSICAL_MATERIAL_NAME.
Notes and References
https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200507135732916.whatsnew/html/xid1927491Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NX_SHEET_METAL
Version: V1953
Function: PREFERENCES
Ref: 002-8559759