NX Sheet Metal Material Attributes

2021-10-06T23:28:03Z
NX for Design

Summary


Details

Ability to use specific Sheet Metal Properties to create NX Attributes

Solution

Since NX12, the Sheet Metal Material Table has been enhanced with the ability
to add specific properties that will create an NX Part Attribute.

Two examples are given by default in ./UGII/materials/sheet_metal_material_table.txt
DRG_NAME and DRG_BEND_RADIUS.

Once a Material is selected in the Sheet Metal Preferences, the corresponding attributes will be created
in the part file as seen below:



Notes and References

https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20190529153536917.nx_sheet_metal/html/xid683639



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NX_SHEET_METAL
Version: V12.0
Function: PREFERENCES

Ref: 002-8559749

KB Article ID# PL8559749

Contents

SummaryDetails

Associated Components

Sheet Metal