NX
Export Assembly from Teamcenter appends part names of the exported parts.
2021-10-06T23:28:03Z
NX for Design
Summary
Details
In Export Assembly from Teamcenter, Naming Rule "${DB_PART_NO}" is being used. A part file revision is selected, which is having wave-linked geometry. This results in the listing of name-only parts including its earlier revisions. Due to this, to assign unique names, NX appends "_1" to the actual part name. This results in changing the actual part name of the exported part to "PartID_1". Since this is appending the actual exported part name, (rather than the name only Parts), this is not the desired result.
Solution
Export Assembly from Teamcenter is listing the earlier revisions of the selected part file since "Allow Multiple revisions" is enabled. So to avoid this behavior, disable the below setting in Customer defaults.
Hardware/Software Configuration
Platform: INTEL OS: windows OS Version: 1064 Product: NX Application: NXMANAGER Version: V1980 Function: CLONE_EXPORT