How to get constraint reaction forces in Solid Edge Simulation.
2021-10-06T23:58:50Z
Summary
Details
Cannot see the reaction Forces.
Solution
Constraint force can be toggled in the Simulation Study. They are not turned on by default to reduce output quantity: The Constraint Forces can then be accessed via the Data Selection (i.e. T3 Constraint Force) . Then you can use the Probe command to select either nodes or faces.
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: n/a Product: SOLID_EDGE Application: SIMULATION Version: V221.0 Function: SOLVE