Fixed Contour operation does not completely machine selected area
2021-10-06T23:28:02Z
Summary
Details
In older versions of the stepover was applied was defined 'On-Plane' We have now changed this to default to 'On-Part'. This may have the effect of changing the toolpath when regenerated in a higher version
Although 'On-Part' generally gives a better toolpath, it may result in the surface not being completely machined.
Solution
The 'On-plane' stepover can still be enabled in later versions by setting a customer default:
Manufacturing - Operation - 'General tab' - 'Allow On-plane Stepover Option in Area Milling' :
restart NX, then edit the operation, you will see the 'On-plane' option is available to be selected in the operation:
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: n/a Product: NX Application: CAM Version: V1980 Function: SURFACE_CONTOUR