About the default customer level "Package"

2021-10-06T23:28:02Z

Summary


Details

From NX 1926 onwards, In NX Viewer, the default customer level "Package" is displayed.


Solution

"Package" level consists of packaged product-specific settings.
Package level settings are designed to override base NX defaults for packaged products like NX Viewer and Simcenter.
UGII_PACKAGE_DIR is not supposed to be changed by customers as it is specific to the Package which allows it to customize NX settings.
Like normal CDs (Customer Defaults), Package level defaults can be overridden by the users if the CDs are not locked at the package level (Normally they are not locked at this level). 
The same rules apply here for the overriding package level defaults as for other levels in customer defaults.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V1980
Function: CUSTOMER_DEFS

Ref: 002-8559304

KB Article ID# PL8559304

Contents

SummaryDetails

Associated Components