Visual Flow Creator execution time

2021-09-03T18:55:38Z

Summary


Details

The duration time of my nodes does not add up. How is duration time calculated?

Solution

Visual Flow Creator calculates the duration time, also known as the execution time of your flows in milliseconds. The duration starts when the flow begins and ends when all the nodes of that flow finish. Time is rounded up to the nearest 100 milliseconds.

For example, you have two flows: FlowA and FlowB. FlowA has 2 nodes and FlowB has 10 nodes. They both start simultaneously, and the duration of FlowA is complete after the second node finishes. FlowB only stops time after the final node, in this case, the tenth node.

You will see the entire flow duration time under inject nodes and function nodes will display the duration for that particular calculation. In addition, you can view the duration time of any flow by accessing the upper right menu and select Flow durations.

For additional examples and optimization tips, visit:

https://documentation.mindsphere.io/resources/html/visualflow-creator/en-US/129229143179.html

Notes

KB Article ID# PL8559192

Contents

SummaryDetails

Associated Components