3D Publishing - how "Create Button" command operates

2021-10-06T23:58:49Z

Summary


Details

In 3D Publishing is possible to use the "Create Button" command, the customer asks how it works specifically by selecting the "Execute Program" option.


Solution

The "Create Button" command operates as follows:


  • Click on the "button" icon on the insert ribbon
  • Drag to select the area to place the button
  • Select the desired action from the pull down menu
  • Setup action properties (if any)
  • Press OK
 



 
Regarding the "Execute Program" action.  This action is NOT recommended for use in HTML web pages.  Most web browsers will prevent the execution of an .exe file from a web page.  Instead, users should use the "Hyperlink to Web" action.  
If the user wants to open a local file, just enter the name of a (non executable) file that will be in the same folder as the HTML file rather than a full URL.  
The "Execute Program" action is included primarily for compatibility with some older files.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: TECH_PUB
Version: V221MP7
Function: 3D_PUBLISHING

Ref: 002-8558903

KB Article ID# PL8558903

Contents

SummaryDetails

Associated Components