Customizing the Generic Motion Operation to include the Reference Subop

2024-06-19T14:42:45Z

Summary


Details

To be able to Loop a Generic Motion operation a Reference Subop command must first be added. This subop is not available by default. How can it be added under the Move Type pulldown?


Notice that there is no Reference Subop between Notes and Conditional Move


Solution

To add the Reference Subop preform the following steps.

1. Create a Generic Motion operation.

2. Select the operation followed by Object and Customize


3. Expand the Explorer, Strategy and the Sub-operation Manager


4. Select Reference Subop followed by Customize Sub Dialog.


5. Enter the Label text, press Standard Parameters, Add to Dialog and OK.


6. Open the operation, press Strategy, Add and select the Reference Subop.


The Loop command can now be added under the Reference Subop.

Notes

For complex tool motion try using the Generic Feature Operation first.

KB Article ID# PL8558102

Contents

SummaryDetails

Associated Components