NX How to represent a hole callout for RH and LH threads in the view

2021-10-06T23:28:02Z
NX for Design

Summary


Details

In a view, the right and left thread should be visible as a callout.

Solution

Example:

In a component is a block with two thread holes (left and right thread) This view is displayed as a section view on the drawing.

The edit function of the view takes you to the "Hole and Thread Callout Settings".

Here is a point in the parameters : "THREAD Direction"

If the thread is selected and the callout parameter is set to THREAD Direction - (RH for Right Hand or an LH for left Hand)
then the Callout will appear in the callout description.

Please notice the Screenshot






Hardware/Software Configuration

Platform: na
OS: n-a
OS Version: n-a
Product: NX
Application: DRAFTING
Version: V1980
Function: DRAWING/VIEW

Ref: 002-8557815

KB Article ID# PL8557815

Contents

SummaryDetails

Associated Components

Drafting