Measure command stops working

2021-10-06T23:28:02Z

Summary


Details

Measure command stops working after launching the Modeling application from Manufacturing


Reproduced Step:
1. Start NX 1980
2. Launch Manufacturing 
3. Execute Measure command ( Measure command dialogue comes up normally at this time.)
3. Launch back to Modeling
4. Execute Measure command

*** No pop up the dialogue.

Solution

The issue is fixed in NX 1984 and NX 2007 Series.


Workaround:
1. Restart NX.
2. Executing the command in Manufacturing.

Notes and References

The problem happens if executing Measure command by going back to Modeling after executing Measure command in Manufacturing. The phenomenon is occurring in all environment other than Modeling such as Sheet Metal, Shape Studio, Drafting or etc.) as well.

*** Please refer to PL8557757 for Japanese article.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1980
Function: INFO_ANALYSIS

Ref: 002-8557758

KB Article ID# PL8557758

Contents

SummaryDetails

Associated Components