Insights Hub Network scenarios for MindConnect Nano and IoT2040

2021-09-07T11:18:58Z
Connectivity

Summary


Details

How to connect your MindConnect Element device to your network.

Solution

When adding your MindConnect Nano or IoT2040 to your network, there are two ways. One, where each of the network ports X1, X2 are going to separate switches or routers. Two, where both network ports connect to the same switch or router. Regardless of the scenario, it is essential to make sure X1 and X2 are not in an overlapping subnet. 

If your network has a gateway, remember that the MindConnect Element devices only route to the gateway on the same subnet. For visual diagrams with IP address examples check out:

https://documentation.mindsphere.io/resources/html/getting-connected/en-US/123470089227.html

Notes

KB Article ID# PL8557469

Contents

SummaryDetails

Associated Components

MindConnect IoT2040 Configuration MindConnect Nano Configuration