Solid Edge Importing STL file in Solid Edge some facets are missing

2021-10-06T23:58:46Z
TRANSLATORS

Summary


Details

When the user tried to import in Solid Edge a STL file the result is not correct, some facets are missing.



Solution

This problem gets fixed with a work around editing the configuration file SESTL.ini (Preferences/Translator folder).

Work around: 
Set minimum facet value to 50 in SESTL.ini.
"Minimum facet number=50"


KB Article ID# PL8557031

Contents

SummaryDetails

Associated Components

TRANSLATORS: OTHER