Cannot export an image to be mapped to a face such as tif or jpg into VRML
2021-10-06T23:28:02Z
Summary
Details
I made use of Decal Sticker command to map an image ( of tif or jpg) to a face and exported it to VRML (.wrl) file. After that, I checked it with a third-party viewer, but I could not find the mapped image anywhere. I could not also find it out in NX even though I imported it back to NX as well.
Step to reproduce: 1.In Advanced Studio environment > execute Decal Sticker command 2.Choose an image file such as tif or jpg as Choose Image File. After that, select a face as the Target. 3.File > Export > VRML 4.Check it with any viewer soft (or import it back to NX).
Solution
It's working as designed. Currently, exporting the mapped image to a face by VRML command has not been supported.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: ASSEMBLIES Version: V12.0.2 Function: PART_FILE_OPS