RobotExpert Controllers for 7R_AXIS_INVERSE, ABB_RAPID, CLOOS_CAROLA, COMAU_PDL, DEFAULT, ...

2021-10-07T00:17:17Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that RobotExpert controllers for "7R_AXIS_INVERSE, ABB_RAPID, CLOOS_CAROLA, COMAU_PDL, DEFAULT, DENSO_PACSCRIPT, EPSON_SPEL, FANUC_RJ, HHI_HRBASIC, IGM_INS, KAWASAKI_AS, KUKA_KRC, MITSUBISHI_MELFA, NACHI_SLIM, NC_CODE, OLP_TOOL, PANASONIC_CSR, ROBOTIC_PARAMETERS_VIEWER, STAUBLI_VAL, UNIVERSAL_URSCRIPT, YASKAWA_INFORM"
are available for download from https://support.sw.siemens.com.

See RobotExpert_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'OLP Change Logs' folder directly under the 'RobotExpert Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'RobotExpert Robot Controllers'
- Select 16.1.1

Download the file(s):

    RobotExpert_16.1.1_7R_AXIS_INVERSE_64BIT_v1.1.13_09_04_2021.exe
    RobotExpert_16.1.1_ABB_RAPID_64BIT_v4.0.2_16_06_2021.exe
    RobotExpert_16.1.1_CLOOS_CAROLA_64BIT_v2.24_09_06_2021.exe
    RobotExpert_16.1.1_COMAU_PDL_64BIT_v4.12.1_09_06_2021.exe
    RobotExpert_16.1.1_DEFAULT_64BIT_v2.88_29_06_2021.exe
    RobotExpert_16.1.1_DENSO_PACSCRIPT_64BIT_v2.28_09_06_2021.exe
    RobotExpert_16.1.1_EPSON_SPEL_64BIT_v2.16_09_06_2021.exe
    RobotExpert_16.1.1_FANUC_RJ_64BIT_v3.16_29_06_2021.exe
    RobotExpert_16.1.1_HHI_HRBASIC_64BIT_v1.5_09_06_2021.exe
    RobotExpert_16.1.1_IGM_INS_64BIT_v1.45_09_06_2021.exe
    RobotExpert_16.1.1_KAWASAKI_AS_64BIT_v4.15.2_17_06_2021.exe
    RobotExpert_16.1.1_KUKA_KRC_64BIT_v5.0.1_30_06_2021.exe
    RobotExpert_16.1.1_MITSUBISHI_MELFA_64BIT_v0.20_09_06_2021.exe
    RobotExpert_16.1.1_NACHI_SLIM_64BIT_v4.29.1_09_06_2021.exe
    RobotExpert_16.1.1_NC_CODE_64BIT_v2.6.14_11_06_2021.exe
    RobotExpert_16.1.1_OLP_TOOL_64BIT_v15.8.1_27_03_2021.exe
    RobotExpert_16.1.1_PANASONIC_CSR_64BIT_v2.20.1_11_06_2021.exe
    RobotExpert_16.1.1_ROBOTIC_PARAMETERS_VIEWER_64BIT_v1.1_14_04_2021.exe
    RobotExpert_16.1.1_STAUBLI_VAL_64BIT_v4.1_11_06_2021.exe
    RobotExpert_16.1.1_UNIVERSAL_URSCRIPT_64BIT_v5.3_29_06_2021.exe
    RobotExpert_16.1.1_YASKAWA_INFORM_64BIT_v5.30.2_22_06_2021.exe



To Install:

Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the RobotExpert installation).

Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

SFB-TECNOMATIX-8554622
Product Information:
  • Product: TECNOMATIX , Application: ROBOTEXPERT

KB Article ID# PL8554622

Contents

SummaryDetails

Associated Components