In NX CAM, how to convert Explorer to Non Explorer dialog Box.

2021-10-06T23:28:02Z

Summary


Details

The versions from NX1899 and above of NX CAM have Explorer type of view for Operation Dialogue Box. Need to switch to Non Explorer Type of Dialog Box which is available in versions prior to NX1899.

Explorer Type

Non Explorer Type:


Solution

1. To change the view, user can use the command "Customize From" by Selecting the
Operation -> MB3 -> Object -> Customize From and select pre NX1899 (Older version) template as shown below.
(E.g:m
CAM_metric_template.prt, library_dialogue.prt, mill_planar.prt, mill_contour.prt)

2. If you need to change the Dialog Box permanently , you need to open the Template files and use the step 1 and save the template file.

3. Alternatively, You can change all/required operations dialog in a part and save that part as template and using that template part for further parts will always give Non-Explorer type of view.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1973
Function: OPERATION

Ref: 002-8554375

KB Article ID# PL8554375

Contents

SummaryDetails

Associated Components