Details
Want to change the name of UGPART dataset name from NX
Once the UGPART is saved from NX, UGPART dataset name can't be modified.
Solution
Add below Attribute Mapping :
{ Dataset type="UGPART"
# (hard-wired) DB_DATASET_ID : "Part File ID"
# (hard-wired) DB_DATASET_REV : "Part File Rev"
{ Item type="Item"
"Dataset Name" : object_name /master=both /description="Dataset Name"
}
}
Start TC and NX
1. Create a new part from NX
2. Add drawing for the above part and save
3. From Assembly navigator select Drawing part -> MB3 -> Properties
4. Now modify the UGPART dataset name under Attributes Tab
5. Save the part file.
Now you can observe , UGPART dataset name is modified in Teamcenter and NX.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1946
Function: ATTRIBUTES
Ref: 002-8554247