Solid Edge Unable to delete breaks in sheet metal bend.

2021-10-06T23:58:43Z
PART/SHEETMETAL

Summary


Details

Unable to remove breaks in sheet metal bends. 



Solution

 The breaks are not able to be deleted when selecting the individual faces due to some small surfaces (slivers). If the break is fence selected the small surfaces are pick up and the break can be deleted then. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1507
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V221.0
Function: FEATURES

Ref: 001-10093651

KB Article ID# PL8553882

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN