How to set the default color of the Parts List template.
2021-10-06T23:28:01Z
Summary
Details
If the border color is defined as Black in the Part list template file, the borderline of the created part list is turned to other colors while using the template.
Refer to the below image [Border colors are not a Black]:
Solution
Solution: ------------ 1. Open template part file. 2. Goto: Menu>Preferences>Drafting>Table>Common>cell. Set Border cell settings as a Black. 3. Delete existing Parts List. and create a new one. Note: [existing part list preferences can not change, we need to create a new parts list.] 4. Save the part file. 5. Use part file as a template. it displayed all cells as Black. ---------------------
Refer to the below image [Border colors are a Black]:
Notes and References
10092943
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DRAFTING Version: V1953 Function: TABLES