What is the reason model not displayed in 3D PDF as fit?
2021-10-06T23:28:01Z
Summary
Details
What is the reason model not displayed in 3D PDF as fit?
The 3D PDF model view is not centered or displayed while opening it in Adobe Reader. we need always Adobe reader to right-click-> Full-screen multimedia to display the model in view.
Solution
In 3D PDF always views are displays the same views as displayed in NX. This issue mostly occurs when the Display View Scale is set other than the Fit method in NX.
Refer below image for more info. Solution 1: ==========
Set Display of the View Scale as Fit from the NX Customer Defaults settings.
If don't want to change Customer Defaults, refer solution 2.
Solution 2: ==========
In NX fit the model in a view and save the views, as shown in the image. and create a 3D PDF, which displays the model in view.
Note: Save option is displayed only for active Views, so active view and save it.
Notes and References
10088057
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: xp64 Product: NX Application: TECH_DATA_PKG Version: V1953 Function: PUBLISH