Solid Edge SQL Server setup failure

2021-10-06T23:58:42Z
APPLICATION

Summary


Details

When installing Solid Edge Standard Parts, the SQL Express prerequisite fails to install. You might see an error message stating: 

"Method not found:'Void Microsoft.SqlServer.Chainer.Infrastructure.RoleService.Intialize 
(Microsoft.SQL.Chainer.Product.RolesType)'.






Solution

This can happen when the SQL Server install path is too long. By moving the setup files to a new folder the error can be avoided. 


In order to see the specific SQL failure you can extract the SQL Express installation from SETUP.EXE. When you manually perform the SQL Express install it will show a list of items to validate. In this case the Path name was too long and caused the installation failure. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V221.0
Function: STANDARD_PARTS

Ref: 001-10092816

KB Article ID# PL8552322

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS