About Refraction setting of Material Editor

2021-10-06T23:28:01Z

Summary


Details

How to adjust Refraction or Index of refraction(IOR) settings when NX_RTS_IRAY = 1




Solution

There is a control on the View Preferences dialog to control this. On the View tab, go to 'More' and select 'Preferences'. Now select 'Studio Rendering' from the list on the left. Now you can select the 'Editing Mode' The default is 'Basic' and this reduces the number of attributes that can be changed. If you change it to 'Full' you now have access to all of the attributes, including 'IOR'.


When you edit the material and find 'IOR', placing your cursor over 'IOR' will display additional help on the setting.




Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10-1909
Product: NX
Application: SYSENG
Version: V1980
Function: VISUALIZATION

Ref: 001-10076603

KB Article ID# PL8552314

Contents

SummaryDetails

Associated Components