NX How to create a gap between edges of flanges

2021-10-06T23:28:01Z
NX for Design

Summary


Details

The ' Sheet Metal from Solid' feature will only joint two edges of the flanges. There is no way to make it leave a gap:


Solution

This must be done individually on each corner by adding a 'Closed Corner' feature:

Note that 'Help' states that we cannot directly add corner relief in the 'Sheet Metal from Solid' feature:




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1507
Product: NX
Application: NX_SHEET_METAL
Version: V1953
Function: SM_FROM_SOLID

Ref: 002-8552152

KB Article ID# PL8552152

Contents

SummaryDetails

Associated Components

Sheet Metal