How to the check part history information without opening part file?

2021-10-06T23:28:01Z

Summary


Details

We check the part history information after opening the part file as the below steps.

Information --> Part --> Part history.

How to the check part history information without opening part file?





Solution

The "ug_inspect" utility can be used to directly query .prt files (From the Installation directories).
Open an NX command prompt and use the syntax: 
 ug_inspect -feature_toggle_info -drive:\path\filename. prt


e.g.  D:\nx****\NXBIN>-feature_toggle_info- D:\working\client_abc\*****.prt


This will return a lot of information, including the full part history with the last version of NX that saved the file. There are quite a few command line arguments for this utility as well. 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: xp64
Product: NX
Application: GATEWAY
Version: V1953
Function: OPEN_NX_PART

Ref: 002-8552057

KB Article ID# PL8552057

Contents

SummaryDetails

Associated Components