Script error in hosted AWC in Open dialog

2021-10-06T23:58:42Z

Summary


Details

When opening a file via hosted AWC, a Microsoft script error is displayed. 



Solution

The client must be on Solid Edge 2021 Maintenance Pack 6 or higher to address Microsoft Internet Explorer browser script errors. When you first activate Solid Edge with Embedded Client and go to the AWS hosted interface, you will be prompted to use Microsoft's Chromium based Edge browser. At the time of opening this browser you will prompted to install the Microsoft add-in browser app, Webview2 / Evergreen. Embedded Client will check for the add-in and prompt with a link to install if it is not loaded; We also check for the right version of Microsoft Edge and how to update if needed. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10-1909
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221MP6
Function: SEEC

Ref: 001-10088610

KB Article ID# PL8551972

Contents

SummaryDetails

Associated Components